This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Automotive - DC DC Converter Module

Other Parts Discussed in Thread: LM5576-Q1, LM5160-Q1

Hi Texas 

we are looking for DC DC Converter Module with below specifications

Input Voltage Min - 36V

Input Voltage Max. - 65V

Output Voltage - 15.6V (adjustable preferred) 

Output Current - 1.5A

Could you please suggest suitable modules as couldn't find in the website, your help will be very useful in selecting suitable module.

  • Hi Hemalatha,

    Are you referring to a module with integrated inductor? If so then there is currently no automotive qualified power module in the TI portfolio.

    If you are looking for a automotive buck converter perhaps you should look at LM5576-Q1 or the LM5160-Q1. 

    Regards,

    Jimmy