This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unique Power Supply

Other Parts Discussed in Thread: TPS55165-Q1

 

My unique power supply/converter basic specifications look like this::

Input voltage:   12Vdc or 24volts AC or DC

Output:  12Vdc @ 1 amp, with operational voltage of -40° to +70°C

This needs to be an extremely small form factor, something that could be used as an inline power module. 

If there are any devices in the ti line up you believe would meet our specifications please share them with me.