Tool/software: WEBENCH® Design Tools
I am using WEBENCH to run a simulation. The condiiton is Vin 4.75V~5.25V, output is 33V/10mA. But it shows an error to suggest to change the input range or change another part. If I change the output to 33V/20mA, the simulation can run correctly. Does it casue any problem if the 33V load is quite small? Actually I have built the board to run this applicaiton, I just would like to run the simulation to conifrm the design. Thanks.