This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2394: Request the Design Calculator Tool

Part Number: TPS2394

Hello

I need Design Calculator Tool of TPS2394.

I'm not found the Calculator  Tool on TI Site.

Could you Provide Design Calculator Tool of TPS2394?

Best Regards

  • Hi Han,

    Unfortunately, we don't have design sheet for TPS2394. The TPS2394 is an older di/dt based current regulation mode for inrush control.  It does not provide FET SOA protection and is intended for low power (<250W) and low output capacitance (<150 uF) applications. If Cout is large (like what would be on a high power output). It is recommended you look at the new TPS23521 instead. It has a much more advanced inrush control (and a very advanced SOA control) that can handle higher power and higher Cout conditions.

    Let me know if you have further questions.

    Best Regards, Rakesh