This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28220: DC PWM 4 phase 3kW boost converter

Part Number: UCC28220

hi Team,

my customer has a quick question that if they can use 2 UCC28220 together for 4 phase 3kW boost converter

if 2 UCC28220 can be operate as synchronous 4 phase boost 

Thanks

4-phase or 6-phase bi-direction DCDC Converter
Normal Direction(Boost Mode) :
    Input : 30~48V
    Output: 48V / 3kW
Reverse Direction(Buck Mode) :
    Input : 48V
    Output: 30~48V / 300W