Other Parts Discussed in Thread: UCC28C45
Hi,
I'm working on a development of a specific power supply (I have chosen a Flyback topology) my specifications are as follows
1. Four Output Isolated
1. Input Voltage : 10VDC-400VDC
2. Output Voltage: 20VDC in each output
3. Output Current : 0.016A in each output
4. Response time of my power supply should be shorter than possible (less than 600us)
Can I use the UCC28704 with primary side regulation for that ? It is possible to eliminate the soft start of the UCC28704 in order to start-up faster as I can ?
Pls do the needful.
Best Regards,
D.SAID