Other Parts Discussed in Thread: UC2902, UC2907, UC3902
I'm designing a load sharing supply with the 29002. I've read through many posts and looked at lots of app notes and diagrams. What I don't understand is how the 29002 can operate with the ground referenced to the load through a sense line type of connection. I'm operating with a low side current sense and if you were to connect the IC ground to the connection at the load, wouldn't this imply that the CS+ and CS- pins are then naturally biased below ground? In the 29002 datasheet it states that the CS inputs have a common mode range that 'includes' ground, but in a remote sensed application those pins would be forced below ground. I see in the datasheet that the pins have a minimum absolute rating to 0.3V below ground but this just seems to be a rating to prevent damage to the IC.
In my prototype circuit each power module is referenced locally to the "-" side of the sense resistor. The power modules when sharing a LS bus are referenced each to their individule ground. I understand that offsets between grounds will lead to sharing errors, but I have had no success in referencing each ground circuit at a remote point at the load. The loadshare bus no longer seems to respond to a changing load current when referenced remotely to the physical load. I have come to the conclusion that both the cabling drops and the sense resistor drops place the CS pin voltages below the IC ground and can no longer properly sense the current sense voltages.
I have read through a powerpoint presentation where towards the final slides it is pointed out that the range of CS pins is -0.3V and in the next slide that the absolute limit is -0.3V.
In my design I have 28V outputs carrying up to 40 amps each module. The sense resistor is a low side 0.002 ohm resistor with kelvin connections. I can provide more detail as to the connections that I'm trying to experiment with.
Just to reiterate the real question:
What is the common mode range of the CS pins?