Due to the limitation of PCB area, and in order to reduce power consumption, I have made changes to the application of lm5116. Please help me to see 1. Whether the chip can work normally when the UVLO pin is directly connected to the capacitor? I am not going to use the UVLO function, so if the capacitor connection will affect the chip work, then the correct way is? 2. Are other connections in the circuit correct?