This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8867-Q1: whether it has risk if Vin is 6-16V, and Vout is nearly 10V

Part Number: LP8867-Q1

Hi Team,

My customer now consider to use LP8867. But 8867 is boost topology.

In  their application, the screen is only 3.1 inch, has 1 channel for 3 LEDs. the total current is 250mA. Vin =9-16V and Vout =10V.

If using 8867, the boost, when Vin =9V and Vout =10V, whether it will have problem or risk?

thanks!

If only consider buck topology, which device do you recommend?