This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65233: PMIC device selection

Part Number: TPS65233

Greetings,

I want to select a suitable PMIC for my product, but I cant seem to find the exact match.  

I have a single 3.7V battery, and an external 5V charging source,

and I need to operate from the battery and provide at least 1A at 3v3,

and then around 500mA on 1v8, and 500mA on 5v, the battery management can be separate as that is the current approach,

but I want to consolidate having the single boost chip and dual LDOs into a single chip if possible

Thank u.

Regards,