This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61052: Minimum Vf of LED in current control

Part Number: TPS61052


Hi team,

1. If the LED Vf is about 2.3 to 2.6V, is it possible to control the current?
2. Can it be controlled no matter how small VF is
3. Are there any disadvantages or points to note in using when Vf is small?

Beat Regards,
Tom Liu

  • Hi yang,

       1. The device also implements a linear low-side current regulator to control the LED current when the battery voltage is higher than the diode forward voltage.

       2. Yes, but the thermal is the main concern if VF is too small(Like LDO);

       3.  Thermal as I mentioned above.

    BR

    Sean