This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25710: where to connect smart battery pack "T" pin ?

Part Number: BQ25710

Hi Support Team,

Looking at the BQ25710 for smart pack charging system. The pack has 5 terminals, namely; [+], C, D, T, [-] and is SMBus v1.1 compliant. 

If the pack voltage falls below under voltage threshold, the cells are disconnected internally and the pack enters Shutdown Mode and cuts power to the system and MCU.

In order to exit Shutdown mode, a charger has to "detect" the pack and provide "wake-up" charge current.
This is achieved by sensing Safety Signal resistance (0 < Rss < 575 Ohm) via the pack "T" terminal which has a 300Ohms to ground. 


My question, where does the pack "T" terminal connect on the BQ25710?