Other Parts Discussed in Thread: EV2400
Hi,
We've developped a 3S1P battery using the bq40z50-r2 component as a gauge, but sometimes, the battery is "blocked". We do not receive informations from the gauge when it is connected to our charger (a LTC1760), and when we try to connect it with the EV2400, it is not recognized, like the SMBus was not functionnal anymore.
We are obliged to do a hard reset (disconnect the cells to stop the gauge alimentation) so that we can recover the communication.
Do you have an idea where it could come from? If you need our configuration or golden files, we can send them to you.
Thanks in advance for your answer.
Best regards,
Renaud