Other Parts Discussed in Thread: TPS2663, STRIKE
Hello everyone
I am using a LM5069 for overvoltage and reverse polarity protecion of a 24V (+-5%) DC input. At the input I have an additional 26V TVS diode for surge protection. My OVLO is at 28V (OVLO low) / 30V (OVLO high). In case of a surge event, the voltage at the input will get much higher than the 26V of the TVS diode and thus higher than the OVLO for short time. Does the LM5069 switch off the MOSFET in this case? If yes, how could this be solved so that a surge event does not affect the circuit behind the LM5069?
Thanks for your help.
Best regards