Hi,
My customer try to turn off BATFET via I2C Register#2 Bit 1 "CE" so that they can measure system current from input. This does not seem to work. Is there some other trick to know? Their HW pin CE is tied to GND via 100K.
Thanks.
B.r M.A.M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer try to turn off BATFET via I2C Register#2 Bit 1 "CE" so that they can measure system current from input. This does not seem to work. Is there some other trick to know? Their HW pin CE is tied to GND via 100K.
Thanks.
B.r M.A.M
Hi M.A.M,
The BQ24250 SYSOFF requires the bit to be set and then input power removed for the BATFET to turn off. It is a true "shipmode" as compared to our other devices that allow you turn off the BATFET any time you want.
Regards,
Jeff
Jeff,
We need to be 100% sure. The term SYSOFF that you mention is associated with Register #6 Bit 4 "SYSOFF"(section 9.6.6) , however the datasheet still in section 9.6.2 describe for Register #2 Bit 1 "CE" and the footnote below, that this BATFET off functionality exist.
- Can you confirm that the datasheet is wrong regarding the ChargeEnable register bit functionality?
Thanks again.
B.r M.A.M
Hi M.A.M,
The /CE pin turns off BATFET current flow from SYS to BAT for battery charging. It does not turn off current flow from BAT to SYS for supplement mode, for example if the SYS load is more than the input power source can provide. Therefore the BATFET cannot be 100% turned off using /CE pin.
Regards,
Jeff
Jeff,
I do not get it.. This is exactly what they want, stopping charging current from SYS to BAT.
The only difference is that you talk about the /CE pin. They tied this to GND via 100K, but instead want to set the Register 2, Bit 1 called "/CE" to '1' by software.
- Can they stop charging current flow from SYS to BAT under this condition? or will the physical /CE pin override the register bit if the pin is tied to GND?
B.r M.A.M