I search DC-DC converter with the following spec.
[DC-DC desired specifications]
INPUT: 24V
OUTPUT: 3.3V, 200mA
Absolute maximum rating: About 50V
Package: SOT-23 (6) is better. (There is no problem to select the other package.)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
If need a ABS with 50V, you need look at parts from BSR-WV product line (>30V). I will move it to BSR-WV.
Hello, please find the product folder LMR36503 and LMR36506.
These devices should fulfill system level requirement, in addition, to being automotive qualified.
If leaded package is required. LMR33610 or LM63625