Dear Sir,
I use the chip to charge the Battery but I'm confusing 2 parameter; V_sys and I_sys.
1: If Vdpm set= 4.5V, Vin=4.7V, what is the V_sys??
2: If Ilim=1A ,Iset= 0.5A and I_bat=0.5A(Changing), what is the I_sys??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
I use the chip to charge the Battery but I'm confusing 2 parameter; V_sys and I_sys.
1: If Vdpm set= 4.5V, Vin=4.7V, what is the V_sys??
2: If Ilim=1A ,Iset= 0.5A and I_bat=0.5A(Changing), what is the I_sys??
Hi Gordon,
Regarding 1, V(SYS)=max of MINSYS or VBAT+~50mV unless input power (VIN*IIN)*efficiency is too low to supply VSYS*(ISYS+ICHG) then the charger goes into supplmement mode and VSYS=VBAT-RDSon*ISYSsupplement.
Regarding 2, the system load pulls ISYS. The charger prioritizes system load over charge current. Maximum output power (VSYS*(ICHG+ISYS)) will be limited by input power =VIN*IIN*efficiency. Assuming you VIN=5V and ILIM=1A, the charger has 5W*efficiency of output power to send to ISYS+ICHRG. ISYS takes priority. Datasheet efficiency curves can help you estimate efficiency for a given VSYS voltage.
Regards,
Jeff
Hi Jeff,
Thanks for your responses quickly.
1: About Vsys, It's variable from 3.5V~4.2V base on the Vbat (Datasheet/ figure 15) does it right??
2: If the Battery energy is full and disconnect the Vin_5v connector, what is the transition time of Vin => Vbattery??
Hi Gordon,
Regarding 1, yes. SYS follows the battery up as it charges.
Regarding 2, the transition time from input power attached to HiZ/sleep mode is in the 10's of us range.
Regards,
Jeff
Hi Jeff,
My english is poor.
"It is in the 10's of us range"; does it 10us ~ 19uS ??