This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5145EVM-HD-20A: modifying the output from 5V@20A to 13V@20A

Part Number: LM5145EVM-HD-20A

Hello.

We are looking for power supply solution with parameters as followed:
- Topology - buck
- Vin = up to 36V
- Vout = 13V
- Iout = 20A

The main requirement is the availability of development board or EVM, because we have a short development schedule.

We found PMP6703 reference design, but the board is not available.

LM5145EVM-HD-20A looks good, but we are not sure this board can handle 13V@20A of load.

Could you please give a recommendation, is it possible to modify LM5145EVM-HD-20A to handle an output of 13V@20A ?
Or if this is not possible, could you please recommend an alternative solution, which does have an EVM for tests?

Thank you.