Part Number: TPS25982
Other Parts Discussed in Thread: LM7480, TPS25940,
Dear Team
I would like to use two TPS259824 devices in power-OR situation from two batteries (as I like the features of this device: very low on-resistance, low on and off Iq etc etc)
Propose to have two identical paths, both paths comprising front-end LM74700 ideal diode controller (for reverse battery protection) followed by TPS259824.
Outputs of TPS259824 are proposed to be connected directly together. Note, one battery will be absent at some times (during hot-swap of batteries)
Would use enable inputs on TPS259824 to turn each path on and off as required (would do this in overlap fashion to ensure power continuity on output, so system would at times be in power-OR situation.
To satisfy spec of max output voltage range of TPS259824, I would propose to add low voltage drop schottky in parallel with body diode in TPS259824 (to ensure Vout is never more than Vin +0.3V when device is switched off)
I'm aware of LM7480 device, but as not available yet in production quantity, so does not seem to be an option for me at the moment.
TPS25940 was also considered for this project, but possibly prefer above solution, as potentially offers a lower on-resistance solution.
Please can you advise if above proposal using dual paths of LM74700 & TPS259824 with connected together output is acceptable please?
Thank you for your consideration in this. James