Hi,
The LM5116 is rated for Vin =100V and an operating temperature range of -40°C to 125°C. I am looking for operation down to -55°C.
I found the LM5116-HT, which expands the range to -55°C to 175°C, but also lowers Vin to 80V.
Is there a version of the LM5116 that will extend the low-end of the operating temperature to -55°C, but still maintain the 100V input rating?
Thanks,
-John