Part Number: LM36922H
Other Parts Discussed in Thread: LM36922, , LM36923H
Is there a dedicated EVM board with the LM36922H on it? Or is the LM36922 EVM the only development platform? Are the two part pin compatible and what are the differences?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi David,
There is no dedicated EVM for LM36922H, and LM36922H isn't a p2p device with LM36922. There are many differences between these two devices, such as boost output voltage range, maximum solution efficiency, I2C selection option and so on.
LM36923H has its own EVM and is compatible with LM36922H except LED channel count.