This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24297: Redetection detects incorrectly.

Part Number: BQ24297

We're using the BQ24297 and have an issue where high power charger can be mis-detected, especially if the charger is plugged in slowly or at an angle. We tried a "force input current limit detection" but VBUS_STAT reports an "Unknown or DPDM detection incomplete" and REG00 remains at 500mA

2 amp charger mis detected After force redetect finish For reference 2 amp charger detected correctly

reg 00 value    32  < Input Current Limit = 500mA

reg 08 value    6c  < 0110 1100, VBUS_STAT= USB host

reg 00 value    32

reg 08 value    2c < 0010 1100, VBUS_STAT= No input or DPDM detection incomplete
reg 00 value    36 < 0011 0110, Input Current Limit = 2A

reg 08 value    6c  < 0110 1100, VBUS_STAT= USB host, I think this should be 'adapter port'
  1. Why is the 'force input current limit detection' failing?
  2. Is it safe to set a higher charge limit if connected to a lower power charger (500mA)

  • Hi,

    1. How did you get column "2 amp charger mis detected" and "After force redetect finish" results?

    2. How did you get column "For reference 2 amp charger detected correctly" results?

    Please also provide the test conditions such as VBUS, VBAT, IBAT, VSYS, ISYS.

    Thanks,

    Ning.