Part Number: UCC27712-Q1
Hi team,
Could you tell me how level shift circuit operates? Could you modify below list if my understanding is incorrect?
Considering input signal "HI" is 0V~10V and high side output signal "HO" is 200V~210V. (HB input is 210V, HS input signal is 200V)
②: Output signal from deglitch filter is 0V~VDD. This filter eliminate non-desired pulse on input signal.
③: Pulse generator output signal is 0V~VDD. It is switching signal for internal SW, that leads to make input signal of pulse filter. the Input signal of pulse filter is 0V~210V.
④: Pulse filter output signal "R" and "S" is in the voltage range of 0V~210V. On the other hand, RS flip flop supply voltages are 200V and 210V.
⑤: RS flip flop output signal is 200V~210V, which is internal switching signal. RS flip flop input signal is 0V~210V from ③、but it could only detect 200V~210V from ④. Input threshold voltage is between 200V~210V (for example, 205V).
From upper list, ③~⑤ operates as level shift circuit, is it correct?
Regards,
Ochi