This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23881: 802.3bt compliance tests

Part Number: TPS23881
Other Parts Discussed in Thread: TPS23882

We are currently testing a configurable Class8 PSE using TPS23881.

We are using Sifos PSA3402 to test the PSE ports.

We have a successful test report at Class8.

But if we limit the ports to other other power classes, then the Sifos test suite report problems.

We would expect the test suite to report failures only when the requested power is higher than the demoted power limit.

But this is not the case. Other failures occur.

We would like to know if the TPS23881 has been tested at other power settings.

EX:

Class8 = Pass

Class7 = Fail at class8 tests

Class6 = Fail so many failures, no report can be generated.

Class5 = Fail at higher classes and some classification tests

Class4 = Fail at higher classes and some classification tests

We are aware that the Sifos PSA 3402 may have some issues with these scenarios, but we would like to know if TI have test reports showing full conformance at these power demotions.

Ou intention is to provide customer specific power limits depending on their available power.

EX: 1 port at BT Class8 and 1 port limited at BT Class4

Thank You

Richard.