This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63060EVM-619: Vout decrease problem on external soft start circuit

Guru 19675 points

Part Number: TPS63060EVM-619

When TPS63060EVM add the soft start circuit by application note slva533(10nF and schottky), large load condition occur Vout dropped.

Please let me know about the reason and measure for Vout decrease.

【Additional information】

・Circuit is based on default TPS63060EVM setting, R2 is only changed 110kΩ to 100kΩ (5.5Vout).

・Iout: 10mA and 60mA are normal 5.5Vout, but 250mA and 500mA are occur Vout drop.

・ Vout drop range is depend on Vin.

・Schottky is tried two type below;

 ・D1NS4

https://docs.rs-online.com/a993/0900766b80fd9a58.pdf

 ・RB521S-30

https://fscdn.rohm.com/en/products/databook/datasheet-nrnd/discrete/diode/schottky_barrier/rb521s-30.pdf

Best regards,

Satoshi