Other Parts Discussed in Thread: UCC39002, , UCC29002, TPS2419
Hello,
thanks for handling this question.
question 1,
I saw on page 17 of the datasheet:
If the frequency source is from the gate outputs of another half bridge controller,interleaving can be achieved.
So, how do I achieve interleaving. Is it only necessary to connect the RT pins of the two controllers and set the RT resistance? Or is there a connection diagram for reference?
question 2,
We want to design a 390 input 24V/1400W DC-DC converter. And use a planar magnetic core to meet the small size requirements. I chose four 350W converters in parallel to achieve. Each converter is designed by UCC28251, and the current sharing is realized by ucc39002. Is there a problem?
Thank you
Thank you!