This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: PRES Pin Hall effect sensor and DC-DC

Part Number: BQ40Z80
Other Parts Discussed in Thread: DRV5032, , LMZM23601

Hello,

We use a Hall effect sensor (DRV5032FBDBZT)  to detect if the battery is plugged in the System.

Is it possible to connect the Output of the Sensor to the PRES pin?
And the Vcc of the DRV5032 to the intern LDO 1,8V from the BQ40Z80?
If yes, at which output is 1.8V?

We also  use a DC-DC 3,3V (LMZM23601) for a MCU, Bluetooth and some LED.
Now I would like to control the Enable from DC-DC via the BQ40z80.

BQ40z80 (Aktiv) -> EN on
BQ40z80 (Sleep) -> EN on
BQ40z80 (Ship) -> EN off

Could you please help me to config the Output Pin to Control the LMZM23601?
Which output should I use and how do I configure it?

Thank you very much!
Thomas