This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2546: Can't charge IPAD AIR 3

Part Number: TPS2546

hi,

The ctr1=ctr2=ctr3=ilim_sel="1", TPS2546 is set in CDP mode.If IPAD AIR 3 is connected, there is no charging current following into IPAD AIR 3. The attache is the DM & DP voltage waveforms when IPAD is connected. would you like kindly help check if there are any errors ? Can you double check if TPS2546 with CDP mode can support IPAD AIR 3?TPS2546-SCH.pdfDP-DM with ipad air 3.xlsx