This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: vs LM74810-Q1

Part Number: LM7480-Q1
Other Parts Discussed in Thread: LM7481-Q1

Hi,

Do you have the comparison table of difference between LM7480-Q1 and LM74810-Q1?

Best Regards,

Kuramochi 

  • Hi Kuramochi,

    Difference between LM7480-Q1 and LM7481-Q1 is the charge pump and DGATE gate drive capability.

    LM7481-Q1 is 5x times higher energy charge pump (LM7480-Q1 features a 600uA charge pump, but LM7481-Q1 features a 3000uA charge pump).

    This enables LM74810-Q1 to perform active rectification of AC superimposed ripple voltage (on battery line) up to 200KHz frequency.

    Basically LM7480-Q1 is recommended for close to 100W (or less) ECU power applications and for >100W ECU applications, LM7481-Q1 is recommended.

    Otherwise, rest of the LM7481-Q1 behaves in the same way as LM7480-Q1.

    Regards,

    Kari.