Hi,
Could you tell me about the frequency of the oscillator(fOSC) and duty.
There seems to be an error between the calculated value and the measured value.
RT=9.1kΩ
CT=1000pF
fOSC (calculated value) = 110kHz
fOSC (measured value) = 122 kHz
*Customers calculate using Formula (3) on page 6 of the application report SLVS074H.
R1=18kΩ
R2=6.32kΩ
RT=9.1kΩ
CT=1000pF
Duty (calculated value) = 49.5%
Duty (measured value) = 44%
*Customers calculate using figure 29 on page 20 of application report SLVS074H.
Are these results reasonable?
Best regard,
Yuto Sakai