Hello TI
I'm using the LMG5200 FET phase leg for a 5A DC/DC converter for high precision current control of magnets in a particle accelerator. My loads are (due to their nature) inductive, ranging from 40 .. 250 mH
Normally, the current is ramped down by control before switching pulses to the FETs are blocked. However, if the control has a problem, switching pulses might be blocked at maximal current (in my case 5A).
The voltage drop over the diode (3rd quadrant) is ca. 3V @ 5A, down to a little bit more than 2V @ 0A, which fits with the datasheet.
This means that I have initially 15 W losses over a diode, dropping to 0W
- within ca. 6 ms for L_Load = 40 mH,
- within 40 ms for L_Load=250 mH.
At project start, the predicted L_Load were around 10 mH, so this was no issue. Recently, the predicted L were increased by more than a decade. So the 3rd quadrant losses in the diode when blocking pulses now becomes an issue.
The thermal information part of the datasheet of LMG5200 has only static (Rth) information, but no dynamic information such as Cth.
Since the chip is rated for 10A, other users might even have higher losses when blocking pulses (I estimate 30..35 W), just probably for smaller times. So probably you already have experience in this topic from other users.
Do you have experience on how long LMG5200 can handle such high losses?
Can you provide dynamic thermal information such as Cth, or Rth as function of the pulselenght or similar?
Best regards
Beat Ronner