Dear all,
I'm not able to find the eqaution to calculate the voltage output in the TPS 40210 datasheet someone can help me?
I need an output of 60V whit an input of 15V
regards
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all,
I'm not able to find the eqaution to calculate the voltage output in the TPS 40210 datasheet someone can help me?
I need an output of 60V whit an input of 15V
regards
David
David,
The TPS40210 controller uses a feedback divider to set the ouptut voltage regulation. The reference at this feedback point (FB) is 700mV (typ) It is specified on page 3 of the TPS40210 Datasheet in the eletrical specifications table under the heading "Voltage Reference"
Equation 57 in the design example on page 30 of the datasheet has the equation to set the values of the feedback resistors Rfb (Vout to FB) and Rbias (FB to GND) for a voltage regulator. It looks like this equation was over-looked in the Application Information section of the datasheet.