Other Parts Discussed in Thread: BQSTUDIO
Hi team,
Could you give me comment on following customer questions? The customer tries to use BQ35100 to monitor the rest of the battery life, and when the battery reaches to the end of the life, BQ35100 sends alarm signal to the host controller. For such use case, the primary battery will be Li-MnO2 and CR type.
Q1. When the battery discharges rarely because the battery operates only when the main supply goes shutdown, can SOH mode be used to estimate the rest of battery life? Or should coulomb counting be used instead?
Q2. For the output of alarm, the customer assumes it is determined after checking the lookup table inside the chip if it is normal or fault. For that case, does the customer need to calibrate the determination threshold of the alarm depending on the battery materials and supplies by themselves? If so, could you tell me how to do that?
Best regards,
Takeshi Sasaki