Hi Team,
My customer is evaluating the UCC27611 by UCC27611OLEVM-203 to drive GaN FET EPC2022. They were advised by EPC that external gate resistance was recommended to be 0 ohm. Under this condition, pulldown impedance is only 0.35 ohm of the UCC27611. On the other hand, absolute maximum rating of sink current (0.5us) of the UCC27611 is 6A (max). Then, they are worried that the peak value of the sink current may exceed the rated value of 6A when turnoff.
How should we consider the sink current peak value when turnoff?
Please advise the criteria the sink current peak value when turnoff.
Thank you.
Best Regards,
Koshi Ninomiya