Other Parts Discussed in Thread: LM51561
Hi TI experts,
Is there a solution that can be designed with the specifications below?
Input : 3.5~8V
Ouput : 30V / 2A & 50V / 1A
I couldn't find a possible solution due to the low input voltage.
Please check it.
Thanks,
Downey Kim.