Hello TI,
We are using BQ24773 Battery charging IC in which we are facing some issues in system development, which is mentioned in below,
1. When Input adapter & battery is connected to the BQ24773 and configure system by using host controller and if input adapter is disconnected but system is ON by battery power after some time we reconnect the input adapter but battery charging is not started, we expecting when input adapter is re-connected to the BQ24773 which running on battery that time it's need to start charging drain battery but it's not happen with existing system need reconfigure BQ24773 again, we don't want to reconfigure system is it possible to it ..?, what we need to ..?
2. We want to monitor battery voltage to avoid over discharge of the battery, what we need to it ..?
Thanks in advance for your valuable support.
Thanks,
Rahul Surawase