Other Parts Discussed in Thread: UCC28070
Hello Team,
This is regarding UCC27524 Driver failure.
We are driving two parallel mosfet using this driver.
Issue is Driver is failed(op short to GND) during load condition.
Without load it perfectly works.PFC output ,we will get 380V without load.
PFC controller IC used is UCC28070 for this application.
choke value is 500uH & CT is 1:200.
Topology used-interleave
Kindly give the suggestion.
Thank you.