Other Parts Discussed in Thread: BQSTUDIO, BQ78350-R1, BQ76930
Hi All :
I have the problems for using BQ76930EVM and please help me to resolve it , thanks.
1. I set the command 0x0011 to ManufactureAccess() by bqstudio softwrae and the discharge current is small than Power : Sleep Current setting.
But the SLEEPM Bit not to set and sleep mode doesn't activate successfully , coluld you have any advice for it ?
2, I want to use BQ76930EVM with BQ76200EVM for protection testing , do you have any document or description for BOQ76930EVM connection with BQ76200EVM (Ex: how to bypass Low side MOSFET
in bq76930EVM )?
In addition, I do the over voltage protection test by using BOQ76930EVM with BQ76200EVM and the COV bit of BQ78350-R1 is trigger , but connector side still has voltage output .
It seems AFE not protection and do you have any advice it ?