This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ21040: Charge current

Part Number: BQ21040


Hi Sir 

May I use BQ21040 for 0.7A charge current ?

I saw the RθJA is 130.8 °C/W ,if the Vin is 5V and Vbat is 3V

The power dissipation is (5Vin - 3Vbat)*0.7A = 1.4W

Tj=25°C+1.4*130.8 = 208.12°C

I think 208°C is too hot ,Have anything I misunderstanding