Other Parts Discussed in Thread: TPS650231
Hi Team,
I am lookding for PMIC which satisfy below requirements:
Output:
1.2V-500mA MAX
1.8V-300mA MAX
2.5V-200mA MAX
2.8V-300mA MAX
3.3V-200mA MAX
Input:3.7V~5V;
Size: within 4*4mm
I find TPS650250 but it can't satisfy size requirement, do you have other recommended device?
thanks a lot.
Best regards,
Yang