This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24725A: ILIM Overcurrent protection (OCP) response time

Part Number: BQ24725A


Hi,

In the D.S. section 8.5.3 "Setting the Charge Current", it describes two forms of overcurrent protection (OCP).  The first one is determined by the charge current register setting and is cycle-by-cycle (6A, 9A, 12A).  The second OCP is determined by ILIM set by external circuit.  Is ILIM considered cycle-by-cycle protection or is it more real-time?  Is ILIM OCP faster than than the first cycle-by-cycle OCP?

-Kelvin