Other Parts Discussed in Thread: LM3409HV, LM3409
I received the LM3409HV EVM and did some quick tests to make sure it was working okay,which it was.
I then replaced R6 for a 30k resistor and R9 for a 82m resistor. After switching the EVM on I didn't get the expected 36.5V output (with load connected), I measured 48V (Vin) instead.
I then reverted the parts back to their original values, but still no result.
As a last resort I tried replacing the IC, but still didn't get the expected voltage output.
It seems as if the EVM is working at 100% duty cycle because when I change the load, the current supplied by the EVM also changes.
I removed the pfet from the EVM and tested it independently and it seemed to be working fine as well.
What is really puzzling is the fact that I can't see any oscillation at the gate of the PFET.
I have also noticed another result which I still haven't found an explanation...The voltage at the VCC pin sits at 42.5V (for 48 Vin). I replaced the capacitor connected between Vin and VCC,but that had no effect.
The reason I mention this is odd is because the VCC pin max rating is 7V.
It would be really helpful if there was a free spice model, or webench simulation, that I could use for reference of working behaviour.
My goal was to have the driver designed such that I could have a 36.5V / 3A (max) output with a ILpp ~ 150mA.
Any advice/ suggestions are welcomed.
Thanks.