Hi, from datasheet of TPS3828-33 I can se that t_out is specified between 0.9s and 2.5s in the whole temperature range? I cannot see any figure specifying the behavior in temperature of this timing. 0.9s is the timing at low temperature or at high temperature? Do you have any timing diagram in temperature?
Thanks in advance for your help.
Best regards.