I'm unable to get an EV2300 box, to be used with the bq77PL900EVM, to stay connected properly via USB. Host OS is Windows XP in a virtual machine under VMWare Fusion. I've been successfully running an MSP-FET430UIF in the same environment, and I believe one of the two drivers the EV2300 uses is also used by the MSP-FET430UIF because the first time I plugged in the EV2300 and it asked to search for a driver, it said that it found a newer one already there. I assume that it was installed for the MSP-FET.
Anyway, I don't know what to do next. I'd love to uninstall the USB drivers fully and try starting from scratch, because I was never asked for the second driver for the EV2300, which apparently comes from the directory C:/Windows/TI/USB2. Is there someone I can talk to who can walk me through this?
Thanks,
Scott