Other Parts Discussed in Thread: BQ24105-Q1
We are using the BQ24172 to charge a 7.2V NiMH pack, and we have a few questions about the re-charge function, and about the typical charging profile:
- When battery voltage drops below the recharge threshold and a new charge cycle is initiated, how does the charger determine what charging current to apply to the battery? It does not seem to start from the constant current phase of the charging profile (about 1A in our case), but at a lower current (~150mA).
- Our measurements during charging show that, in the voltage regulation phase (Figure 14 of data sheet), the voltage on the battery is not exactly the same but goes up a slight about (maybe 200-300mV as current goes down). Is that correct behavior? How does the charger set the duration for for the current curve in this phase (is it some RC-type exponential decay)? Or is current in this phase based on how close the battery voltage is to the termination voltage set by the FB-pin divider? What will happen if the battery cannot reach the termination voltage because it it set to high for the cells?
Thanks,
Jackson