This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: CB Certificate

Part Number: TPS1663


We want to use TPS16632 with 24V and 3A.

Why is there no CB certificate rating ?

So its not conform with IEC62368 ?

Do you have another solution ?

best regards,

Martin

  • Hi Martin,

    The IEC62368 certification demands 5A current limit or 100W powerlimit which ever is lower.  UL evaluated the device at 20V and 5A which covers both the requirements.  Hence as long as your application uses <5A or 100W, you use the TPS1663 certificate

    Best regards, Rakesh