Other Parts Discussed in Thread: TPS2290
Looking at the TPS22990 to use as a controlled switch for 3.3VDC and 5VDC. I noticed in the datasheet that it recommends an input to output capacitance ratio of 10 to 1. So if there was 100uF of capacitance on the output, I would need 1mF of input capacitance. Is there anything specific reason for such a large input to output capacitance ratio? As long as the input voltage stays above the recommended minimum operating voltage during the inrush current and I have less than the 10 to 1 input to output capacitance ratio, are there any issues with the TPS2290 operating correctly?