Hi,
I want to use external power sequence by controlling enable pins of DC-DC converters of TPS65070.
In data sheet, they mentioned that when controls EN pin independently, sequencing program needs to be DCDC_SEQ[2:0] = 101.
Default sequencing of TPS65070 is DCDC_SEQ[2:0] = 011.
So it means that if i use external sequencing then DCDC_SEQ[2:0] register move out of picture ?
If not then how to manage DCDC_SEQ[2:0] ? B'cz TPS65070 will not power ON due to its default register setting.
I need below power sequencing with external control
1.2V (VDDC3) ---> 1.8V (VDDC2) -----> 3.3V (VDDC1)
So let me know that i am able to control DC-DC converter independently through its enable pin or not ?
Thanks,
Hitesh