Hi Expert,
Customer is looking for a solution 5Vin(USB) single cell charger with 300mA charging current(taper 30mA) with OTG, Vsys output(power path), programmable interface, and OVP features.
We are considering BQ25618 but one question regarding OTG would like to clarify with you.
The product would only have one USB typeC port and it could be either supply input or OTG 5Vout.
My questions is when in boost mode, is VBUS also same as PMID voltage e.g. 5V and can we connect accessory on VBUS leaving floating on PMID?
Why I am asking is because I see the statement in DS 8.3.4 that when in boost mode, the Q1 will be off so I am not sure connecting accessory to VBUS is a right way to do.
Would you please provide comments about it? Thanks.
Regards,
Allan