Other Parts Discussed in Thread: BQ40Z80, BQSTUDIO
Hi team,
I'm trying to get BQ40z80 evm functioning, I have the power supply at 8V connected between 1N and 2P with the two 1k res in between. All other connections on the block are shorted. Sys pres pin is connected PACK- on the other block. When I press the wake up button (S1) the with a load connected across PACK+/- the load will see 8V for a short time but then goes to 0V. I think I am missing something here, why is it not able to continuously discharge after pressing S1?
Thanks,